Part Number: TPD1S414
I have a board that we will be testing with a pogo pin interface. The current jig does not allow me to plug in a USB cable to the board and I didn't provide a testpoint between the connector and the TPD1S414 input. The only place the test jig can apply power is to a TP after the TPD1S414. Will there be any issues with VBUS_SYS having 5V on it while VBUS_CON is floating?