Part Number: DS90UB964-Q1
Other Parts Discussed in Thread: ALP
Dear TI Experts,
We are examining the connection 4 cameras in Line-concatenated forwarding of UB964.
(Refer System image)
There is no problem if there are 3 cameras connections,
but if there are 4 cameras connections, the picture does not appear correctly.
(Refer Get image. 3cameras connections:3843x481 4cameras connections,:1025x481)
We have exceeded the Line length specification.
Please tell me the limit of Line Length at Line-concatenated forwarding.
Our environment is below.
・4 cameras connect (1280x480,YUV422,216Mbps/Lane)
・Serializer is UB933
・UB964 CSI output is 1600Mbps/Lane setting
・Output port is CSI-TX0
・VC:0,DT:1F
・Frame Sync mode (Line-concatenated forwarding)
Thank you and best regards,