Part Number: DS90UB936-Q1
Other Parts Discussed in Thread: DS90UB935-Q1,
Hi
I have an application were we plan to use DS90UB936-Q1 and DS90UB935-Q1. Appart from forward channel image data we are planning to transfer data on the back channel in a as high data rate as possible.
I have read the data sheet but for me it's not totally clear how the back channel works.
1. Is the maximum data frequency 416 kHz or can we get 4x416kHz using all four GPIOs.
2. Does 416 kHz mean a bit rate of 416kbit/s or do we have to provide a data enable bit in half speed so we can get maximum 208 kbit/s?
BR
Johan bendz