Part Number: SN75188
Other Parts Discussed in Thread: LT1030,
Hi Sirs,
As discussed before.
Does LT1030 could be used with the SN75188?
We use RS-232 Driver, how do I need to connect ON/OFF and STROBE?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shu-Cheng,
Yes, you can use LT1030 to replace SN75188. Both are RS-232 drivers. You can leave STROBE bar pin open if you don't need to use it. For ON/OFF it's a little bit inconvenient. You need to connect it to a 5V (up to 10V). If you don't have a 5V rail available, you may need to generate a proper voltage from 12V rail. Please let me know if you have more questions.
Regards,
Hao