Part Number: SN65HVD70
Hi Team,
Please help me answer the follow question, thank you so much.
SN65HVD70 IC is used in RS485 secification. The input A and the output Y are connected.
When the DE is set to "L" then the output is high impedance, the level of the date+ line(the input A and the output Y) becomes about 1V.
What is the reason? Does the input A has an internal pullup resistor?
BR
Tom.Liu