This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: RMII slave and master mode of operation

Part Number: DP83822I

Hi,

We are working on a radio product which works in 125MHz band. and hence we have a limitation in our design on usage of 25MHz, 

We are planning to operate DP83822I PHY in RMII slave mode.  The PHY and MAC will be fed from an external 50MHz clock oscillator using clock buffer (1:2).

As per AN-1794 app note (http://www.ti.com/lit/an/snla101a/snla101a.pdf), operating on two separate clocks (in RMII slave mode) might introduce an uncertainty in the latency of the PHY receive datapath.

Is this applicable even when I am using same clock source to feed both PHY and MAC?  We are aware that there is no physical clock connection from PHY to MAC (as in MII  mode) in RMII mode.

If latency is introduced due to this type of clock topology, what is the maximum latency that can be expected in PHY datapath.

Regards,

Archana Rao

  • Hi Archana,

    RMII needs buffers since it doesn't have dedicated transmit and receive clocks. These buffers will introduce variation in latency, even when same clock source is used to feed PHY and MAC. This is due to how RMII standard is implemented. Usually in applications where low variation in latency is required, we recommend using MII interface. Since latency sensitive application do not use RMII, we haven't characterized RMII latency variation for DP83822.

    -Regards
    Aniruddha