Part Number: DP83848C
Hello,
I am struggling to connect my uC (STMF4) to DP83848 PHY. I can read the registers and get the values from them, but when I try to ping it, nothing happens on either RX[0:1] or TX[0:1]. I am using the board in RMII mode. I measured PFBOUT voltages, but now I am stuck. When I connect the cable the led is ON and also pc recognize that something is connected to the board. But from here on nothing works.
I think the problem is on the PHY side, but I don't know if the PHY is broken, or I have to write some special value to some registers to start transmitting the data through?
Thank you for your help.
Regards, Jaka