Part Number: LMH1983
Other Parts Discussed in Thread: LMH1981, LMP7711
Hi,
I have added the LMH1983 and it fails to startup for some reason. There is also an LMH1981 on the PCB connected and it operates fine feeding back a Vsync & Hsync to the LMH1983.
The VCXO is oscillating @ 27MHz.
I can see the PLL1 output sometimes tries to oscillate @ 27MHz for a few milliseconds after powerup but then dies, other times it doesn't have any output at powerup.
I have the option of fitting the LMP7711 but at present the VC_LPF is fed back directly to the VCXO (CTS 357LB3I027M000).
I erroneously omitted adding the CP, CS & RS components to the PCB layout, will this be the issue? I have strapped on the CP = 1uF but still no joy.
Should have stated, I was trying to access I2C registers and the device does ACK but readback always gives 0x2A, I suspect this is the 0x00 register contents and that the address is not being decoded as the 27MHz PLL1 is not running?
thanks,
Paul