Part Number: HD3SS214
Hi,
I am making a 2x2 Displayport 1.4 switch (2 IN, 2 OUT) as shown below:
https://i.imgur.com/vqRvCep.png
In which, I use 2 re-driver at both ends of this switch. I'm confused about the AC coupling capacitors on AUX channel.
Should I implement it at either end or just one side (Sink or Source)?
https://i.imgur.com/T1LWPT2.png
Besides, with the pull up and pull down resistors on AUX channel, is it optional or mandatory?
And which line should be pulled by these resistors ((1) Between Source and SW, (2) Between 2 SWs, (3) Between SW and Sink)?
Thanks and best regards,
Hai