Other Parts Discussed in Thread: DS90UB947-Q1, DS90UB948-Q1,
Hi Sir
I'd like to ask for your help with the following:
- Spec -
LCD : LVDS 2ch left/right mode
CPU : imx6 ( LVDS 2ch odd/even mode)
LCD : 1920*720 12.3inch FULL TFT LCD (LA123WF4)
1. Is there any IC that can convert odd / even mode to left / right mode when outputting LVDS?
2. Imx6 does not support 1920 * 720 when outputting DSI. Is there any IC that changes HDMI or LVDS to DSI?
3. Is there any IC that changes to left / right mode when changing from HDMI to LVDS in HDMI output?
Multiple ICs may be used.