Part Number: DS90UB948-Q1
hello
we use DS90UB948-Q1 in our display product.
Both +/-4KV ESD Contact Discharge test are failure, the phenomenon is that the dispay picture appears to flicker.
When we fix the diaplay panel's backlight enable control pin to Level high instead of controlled by the GPIO 1/Pin 8 of 948, Both +/-4KV ESD Contact Discharge test are pass that has no flicker phenomenon.
So we can confirm that this issue root reason is 948's weak ability of anti-ESD in our system.
we have added TVS on the circuit of GPIO 1, but it has no work.
we also add chasis on the PCBA board, but it has no work.
Could you help provide any suggestions on this issue?
Thanks