Part Number: TPD4S014
test condition:
D+,D- pin;
ESD 8KV,contact,
Vmax clamp=11.1V
Is the voltage ok?
The Absolute Maximum Ratings of CPU's D+/D- pin is 6V,It will damage the CPU.
Can you help to resolve it?
By the way,what's the Vcalmp in the conditon of the following test described by spec?
ESD Performance D+/D–/ID/VBUS Pins:
– ±15-kV Contact Discharge (IEC 61000-4-2)
– ±15-kV Air Gap Discharge (IEC 61000-4-2)