Part Number: TUSB4041I
In the datasheet, I can read the following: "The VBUS detection requires a voltage divider. The signal USB_VBUS must be connected to VBUS through a 90.9-kΩ ±1% resistor and to ground through a 10-kΩ ±1% resistor from the signal to ground." The recommended USB_VBUS voltage at pin 16 should be somewhere between 0 V and 1.155 V according to datasheet, but the actual threshold is not stated. What is the actual threshold (voltage) at USB_VBUS (pin 16) to distinguish between USB_HOST_connected / USB_HOST_not_connected?