This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: how to set Internal Default Timing Configuration?

Part Number: DS90UB948-Q1


hi

We want to set DS90UB948 into Internal Timing mode so it can generate test patterns without FPD-Link III.

Like this:

I only find this file, but it does not contain DS90UB948.  http://www.ti.com/lit/an/snla132c/snla132c.pdf

In Register 0x65,  how to set bit 2?  we don't have any clock or timing source input to 948.

If set bit 2=1,  Do I need set the Internal Timing Default Values ,  as the table 10 listed in the file of snla132c.pad.

If yes,  I can not find the suitable registers to set them.

Thanks a lot!

  • Hello Jesse,

    I am in the process of updating this app note, hoping to release by the end of the month but generally speaking the register configuration for 948 is the same as what is described in this app note. Please follow the example in section 4.3 and set your timing parameters appropriately based on your specific display. 

    Best Regards,

    Casey