Part Number: DP83849C
Dear DP83849C experts,
I am using the DP83849C phy. I understand that there are 3 types of loopback tests available with this phy. They are:
- Internal BIST test. A pseudo random pattern is generated in the phy and looped from the phy internal TX to the phy internal RX and compared.
- External BIST test. Same as internal BIST above, except the loopback is performed with a ethernet loopback plug that is plugged into the RJ45
- PMD test. A test which loops back data received from the physical layer back into the tx path and in turn back to the physical layer. I presume you would need some sort of device/application that can verify the integity of loopbacked data.
I have two questions in relation to this.
1) Is my description above correct ?
2) Is it not possible to loop back data in the phy that it received from the MAC, such that the MAC receives data it transmitted ?
Kind regards,
Rocco