This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125BR820: whether the device can support BANK A connect to 10G-KR and BANK B to X4 PCIE3.0?

Part Number: DS125BR820


Hi team,

Whether the device can support BANK A connect to 10G-KR and BANK B to X4 PCIE3.0? Thanks.

  • Hi Frank,

    Electrically there is no problem with 10G signals on A and 8G signals on B.  The potential problem will be any Rx Detect operations with PCIe signals.  Would this application have to support hot insertion and removal?  If "yes" then there will need to be active SMBus control to reset the Rx Detect circuits on the B-bank signals connected to the PCIe link.

    Regards,

    Lee