Part Number: TCAN4550
Hi Team,
As topic, which block in TCAN4550 is VCCOUT supplied to? Thanks.
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN4550
Hi Team,
As topic, which block in TCAN4550 is VCCOUT supplied to? Thanks.
Andrew
Andrew,
The VCCout block powers the integrated CAN transceiver and has a total current capability of 125mA. It can be used to power an external load, but consideration has to be taken for how much current the integrated CAN transceiver can consume at any given time when calculating the max external load the output can handle.
Does this answer your question?
Regards,
Hi Eric,
Thanks! Please correct me if I am wrong.
VIO supplies the SPI interface, and cannot directly connect to VCCOUT, VIO must settle before VCCOUT, therefore must use separate source for VIO, correct?
Andrew
Andrew,
There shouldn't be an issue tying VCCout to VIO, there isn't any timing requirement on either supply. Was there something you read that said otherwise?
Regards,
Hi Eric,
Maye I mis-understood, so I don't need to follow Figure 15. Power Up Timing ?
It showed VIO settled before VCCout. Thanks!
Andrew
Andrew,
The VCCout timing in that plot is purely based on the timing of VSUP crossing the wake up threshold and the how long VCCout takes to ramp from that time. VIO is powered up at a seemingly random time because it is system dependent, and is only there to show the timing of it ramping up and then the CLKIN signal beginning to work. They are independent of each other.
Does this make sense?
Regards,