Hi team,
Thanks for your support.
I want use TPD1S514 to protect VBUS Protection, I have some concern with it,please help to confirm.
1.If the voltage on the VBUS is 6~8V, Does the TPD1S514 damage?
2.Does TPD1S514 have current limit?
3. I use the TPD1S514 as a device in this application,it's only a UFP, the UFP connect with computer by cable,the input capacitance on VBUS is relative to the inrush current and overshoot when hot swap, I am not very clear whether the inrush current requirements for device in the 2.0 standard? please help to confirm.
4.Could you give me some advice, how much the input capacitance on VBUS can meet he usb2.0 standard? 2.2uF on VBUS of USB, is it OK?
5.Since the package of TPD1S514 is BGA, Is there any other package?If not, please recommend other IC that can be replaced.
Look forward to your reply, thank you.
Kevin