1、Can the Ds90UB933 / DS90UB913 support 1080P@30fps?
2、When the Ds90UB936 is paired with the DS90UB913/933A-Q, does it need a sensor or ISP to output the CSI-2 signal? At present, our output is the BT656 format signal.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、Can the Ds90UB933 / DS90UB913 support 1080P@30fps?
2、When the Ds90UB936 is paired with the DS90UB913/933A-Q, does it need a sensor or ISP to output the CSI-2 signal? At present, our output is the BT656 format signal.
Hello,
913A/933 do not support BT.656 because the format does not contain traditional sync signals. We currently do not have a SERDES combination to support BT.656
Best Regards,
Casey