Part Number: TRS3232E
Other Parts Discussed in Thread: TRS3232, TRS3122E, DS160PR410
Hi Sir,
Could you please help to review below schematic for TRS3232?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRS3232E
Other Parts Discussed in Thread: TRS3232, TRS3122E, DS160PR410
Hi Sir,
Could you please help to review below schematic for TRS3232?
Thanks
Hi Anne,
I reviewed the TRS3232 schematic. Why are there 1-kOhm series resistances on the RIN lines? Generally I wouldn't recommend this since it will cause some loss of signal amplitude. (It will form a divider circuit with the input resistance of the RS-232 receiver, which is typically 5 kOhm.) Other than that, I didn't have any major concerns.
I did see that there was a note that a TVS was not needed on RIN since it can support higher voltages. I wanted to point out that TVS diodes are generally intended to clamp transient over-voltages like ESD strikes, though, not to clamp DC voltages. If you need to protect against higher DC voltages, then you should double-check the TVS capability and if needed implement extra protection. If you are just protecting against ESD, you might see if there is a transceiver whose internal ESD protection is sufficient.
I also noticed you are using level translators to communicate with a 1.8-V IO. You might consider using TRS3122E as the transceiver instead of TRS3232. It can be powered by 1.8 V directly, or it could be powered by 3.3 V and a 1.8-V logic supply can be used. In either case external level translators would not be needed. The TRS3122E also integrates level-4 IEC 61000-4-2 ESD protection on the DOUT and RIN lines, so it may eliminate the need for the TVS diode as well.
Also, did you intend to start a new thread with your DS160PR410 question? If so, you can put it in a new thread by clicking "More" underneath the post and then selecting "Split."
Regards,
Max