Part Number: DS92LV18
Other Parts Discussed in Thread: SN65LVDS100, SN65LVDS101
Hi
I am designing a Ser/DeSer board using the DS92LV18. I have added external logic with latches etc. to create a 64bit point to point multiplexer by using 2 identical boards and connect them with fibers.
I have actually 2 questions I hope someone can help me with.
I have an 25Mhz oscillator on the board. I intend to connect this clock to both the Tclk and the RefClk so that both the Tx side and the Rx side are clocked by the same oscillator.
Is this the correct way of using the DS92LV18?
Secondly I am having a bit of difficulties to find a level conversion circuit. The DS92LV18 has an LVDS interface on the DI+.DO- and RI+ and RI- pins. The fiber component I am using has LVPECL level interface. Can anyone help me with an application note on how to make this conversion?
Thanks in advance.
Regards