This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/DS90UB954-Q1: How to design a fusion camera system??

Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB960-Q1,

Tool/software: TI-RTOS

Hi

I am designing a fusion camera system between visible sensor and infrared sensor

The visible light module and infrared module had different pix clock and different resolution.

According to the application of DS90UB954-Q1 and DS90UB960-Q1, I can use Coaxial cable connecting to FPD-Link III HUB

If I can just Use only one coaxial cable to transfer data of visible module and infrared module?

Do you had same designed demo for this situation?

  • Hi,

    954/960 is de-serializer to receive the video inputs from camera based on different ports, but one port only can receive one camera input signal.

    So for your applications, since you need two cameras, every camera needs one separate cable to transmit the high speed signal to 954/960 with cable.

    Steven