Part Number: SN65LVDS33-EP
I just wanted to confirm that the only way to guarantee a high impedance state at the output is to power the device and disable the output.
-
Is it required to drive both of the enables to put the device in High Impedance at the Output?
-
Can I just toggle the G pin to enable and disable the output?, Do I need to tie the Gbar pin to Vcc in this scenario for operation?
-
If the part is run at a VCC of 3.0V what are the VOH Min and VOL max values?