Part Number: TCA9543A
Hi,
I will like to find out the maximum allowable junction temperature of TCA9543APWR.
Thank you.
Best Regards,
Dawson Yeo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9543A
Hi,
I will like to find out the maximum allowable junction temperature of TCA9543APWR.
Thank you.
Best Regards,
Dawson Yeo
Hey Dawson,
There are two types of Maximum junction temperature: Recommended Maximum and Absolute Maximum.
For Recommended Maximum: 85C is the answer.
For Absolute Maximum junction temperature, i would putting the limits based on the Vcc levels.....
At Vcc>3.6V I would recommend you stay below ~90C
At Vcc<=3.6V You should stay below 105C
Thanks,
-Bobby