This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD75: Searching for a 5V RS-485 device which support the same or smaller package as SN65HVD75

Part Number: SN65HVD75
Other Parts Discussed in Thread: THVD1450

Hi,
My customer used to use SN65HVD75, now they are searching for a 5V device with the same small package size as SN65HVD75. SN65HVD75 can support a "VSON" package. please kindly suggest if we have such kind of device. thanks.
  • Hi Yue,

    The best option is probably to use the newer THVD1450 device.  It is available in the same VSON package as SN65HVD75.  This device can operate at VCC levels from 3 V to 5.5 V, and so you could use a single part number for both the existing and newer applications.  Please let us know if you have any questions on the device.

    Regards,
    Max