This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3410: Check the TUSB3410's connection of VREGEN , SUSP and RESET

Part Number: TUSB3410


I have a question of TUSB3410IRHBT.

I  want to use TUSB3410IRHBT to translate  USB to I2C.

I follow the application note"TUSB3410 USB to I2C Application Note.pdf " to draw my schematic.

However, FAE tell me that the VREGEN , SUSP and RESET are wrong connection.

I want to check them  which connection is right.

The application note shown below:

The FAE suggest us the correct connection shown below:

  • Hi,

    I would recommend following the first schematic from the app note. However, in the second schematic VREGEN/ would see 3.3V after reset is deasserted. Are you going to provide an external 1.8V?  

  • Hi,

    Is there any more support needed for this issue? If so please reply with any relevant details so that I can further assist you. For now I will be marking this thread as "TI Thinks Resolved". If you have resolved your issue, please post the solution to the original problem/post for others with similar issues.