Part Number: TRS3221E
Other Parts Discussed in Thread: TRS3122E
Hi Sirs,
Sorry to bother you.
Does TRS3221E have support UART 1.8V CMOS level?
If no ,should we need to refer TRS3122E? but actually we only need 1 TX/RX.
Thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Shu-Cheng,
No, TRS3221E does not support 1.8-V IO; it is intended for 3.3-V logic levels or higher. For this application TRS3122E would be the better choice. You could leave the unused RIN, ROUT, and DOUT ports floating and tie the unused DIN port to 0 V or 1.8 V.
Max