Part Number: TUSB8041
Other Parts Discussed in Thread: TPS74801
Dear Team,
1.The TUSB8041I have the I2C EEPROM operation and SMBus slave operation mode, however, some parameters can be set by the HW pins, if we select external EEPROM mode, what EEPROM you recommend? There are also have OTP in the usb hub, is it probably programming our configuration before import to Delta?
2.The TUSB8041I need dual power rails (3.3V, 1.1V), there are no specify power on sequence describe in the section 8.3.7, the core power 1.1V we plan use an LDO and TRIM the 3.3V, the both rails probably startup at same time or between very short time, is it acceptable? For the LDO consumption, we have USB 3.0 upstream, one 3.0 down-stream, two 2.0 downstream, can you recommend the proper LDO to us?
3.I saw the USB compliance eye test for each downstream port in the datasheet, what’s the runtime OS for this compliance test? Our CPU is x86 and linux OS, all the downstream USB ports can be test directly?
BR
Kevin