Part Number: DP83822I
Other Parts Discussed in Thread: DP83867IR
Hello, is the strap function able to be set with the MII interface on the PHY of the DP83822I and DP83867IR?
application: Motor Drive
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
Yes, strap functions are indeed assigned to MII pins of DP83822 and DP83867. However, there are other pins like GPIO and LEDs that may also have strap functions. Please refer to respective product datasheet for more information on which pin has strap functionality.
-Regards
Aniruddha