Part Number: DS90UB933-Q1
Hi team,
Customer wants to use DS90UB933 as PCLK from imager mode. In this case, the datasheet describes "MODE pin can be pulled up to VDD_n (1.8V) with a 10-kΩ resistor directly or use the ratio shown in Figure 18 and Table 2.". But, customer wants to connect MODE pin to VDD_n without pull-up resistor.
Is there any impact for system when MODE pin is connected to VDD_n without pull-up resistor?
Regards,
Nishimura