Other Parts Discussed in Thread: TUSB9261
When the TUSB9261 is powered off (3.3V / 1.1V) and the 35/36 pin (USB_DP / USB_DM) is connected to a powered-on host, is there any problem with the pin rating of the device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the TUSB9261 is powered off (3.3V / 1.1V) and the 35/36 pin (USB_DP / USB_DM) is connected to a powered-on host, is there any problem with the pin rating of the device?
Hi,
Is there any more support needed for this issue? If so please reply with any relevant details so that I can further assist you. For now I will be marking this thread as "TI Thinks Resolved". If you have resolved your issue, please post the solution to the original problem/post for others with similar issues.