Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Tool/software: Linux
Hi TI-team
We are using your TPS65987D chip as a USB-PD controller.
First, I have write the eeprom through SPI. After that, I have read the content of eeprom and it is exactly what I want to write.
Secondly, I have powered on all of the input needed(VIN_3V3, PP_CABLE, PP_HV) and I get the output of corresponding pin(VBUS, LDO_3V3, LDO_1V8, C_CC).
Then I measured the SPI signal when reboot the device without platform writing the EEPROM, and there is no SPI signal at all.
So I think the TPS65987 didn't read the eeprom totally and maybe even didn't start to work.
Finally, I tested the function of USB and it can neither work as a host nor work as an charger.
Could you please help me figure out how to operate the TPS65987D to read the eeprom normally and how to check whether the TPS65987D read the flash successfully?
Best regards!
Yi Zhang