This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: I2C address for I2C1 port

Guru 29720 points

Part Number: TPS65987D

Hi Team,

The datasheet shows "Short ADCIN2 to LDO_3V3" to set I2C UNIQUE ADDRESS[3:1] = 011b.



On the other hand, TPS65987EVM schematic shows the following resistor divider (10k/100k) for ADCIN2 as the following.




Which do you recommend to set I2C UNIQUE ADDRESS[3:1] = 011b?
The background of the question is my customer designed their board which ADCIN2 is pull-up to LDO_3V3 through 1kΩ resistor, however a few boards coudn't access I2C1 as expected.

Best Regards,
Yaita