Part Number: TPD2S703Q1EVM
Hello,
I would like to know if it is possible to protect low speed signals such as SMBUs with the TPD2S703Q1.
I have a smart battery with SMBus and I would like to protect the CLK & DATA from short with the 17V battery voltage (in case a short occurs in the cable).
Since I already have TPD2S703Q1 on the board to protect USB 2.0 diff pairs, I wondered if this chip could also be used for single ended signals... I suppose this is possible only if the signals are not coupled inside the TPD2S703Q1.
With many thanks in advance.
Thomas