Part Number: LMH1228
Hi Team
What is the expected value of the input signal level of the LMH1228?
According to the standard, the output level of the previous stage is at 300 to 850mV,but the transmission loss is calculated as -6dB and the input is 150 to 425mV.
Does this mean the assumption of an input voltage of this level?
Why is there no provision for IC input pins?
If you do not know the transmission path, you can not assume what the actual input will be.
As loss of 4 to 5 dB is also assumed, I think that there is a possibility of actually shifting.
Does that mean that the LMH1228 has enough margin to absorb it?
Thanks
Best regards,
Shidara