Part Number: TPS65988
1) If an external source is provided to the VIN_3v3 pin, does the "ILDO_3V3_EX" parameter, listed on Pg.8 of the datasheet still apply? Based on the various datasheet diagrams, I am lead to believe the 25mA maximum strickly applies when the LDO is the source, and no external source is on CIN_3v3 pin. If this is the case, then I suspect there is an upper limit on the current flowing through the switch and thus, what is this upper limit?
2) Also, related to the previous question, and on page 8. There is a bit of confusion on my part and I would like to get some clarification. ILDO_3V3_EX states max current is 25mA, but in the previous 2 parameters, it lists the Current Load as twice that at 50mA. I hope you can see my confusion and can provide some clarity.
3) Finally, I can't seem to find the GPIO Drive Level (aka IOL Low-Level Output Current or IOH High-Level Output Current). My hunch is, this is also related to the above questions, I.e. if using LDO is the source, then combined max is 25mA, but again, does that still apply the one you provide VIN_3v3.,