Part Number: TUSB522P
Hi,
There is a mismatch regarding Control Pin values in the TUSB522P Datasheet and the EVM User Guide (OS and DE values):
This is from the Datasheet (Revised May 2019)
and this is from the EVM User guide (August 2016):
There is a mismatch between OS High voltage (1.1V vs. 1.2V) and also DE-Emphasis Ratio when OS is high (-2.6,-5.9,-8.3 vs. 0,-3.5,-6.2).
It seems like the Datasheet has an error in the DE value since the value seems not to change when OS changes. Regarding OS voltage i cant tell.
Can you please verify the correct values?
Thank you