Part Number: USB-C-PD-DUO-EVM
Other Parts Discussed in Thread: TPS65987D
Dear Team,
My customer is trying to evaluate the USB-C-PD-DUO-EVM with Samsung S10 mobile.
They've ran into the following issues :
- We supply 20v Vin, below 15v the board not working, why?
- Charging current looks sinusoidal on DC – why?
- Vbus is stuck on 5v, push buttons not working, why?
- Is tps65987d come with default parameters for charging?, if yes what are the parameters?
- The GUI is very complicated, how can we work with this GUI?
- How can we work with the GUI\board to work with our project requirements:
- Vin is 12v max
- Vbus is 5v or 9v, depend on Sink requirement
- Icharge is 1.5a or 3A depend on Sink requirement
- No flash to configure tps65987d during start up
Can anyone on the team please support ?
Best regards,
Nir