Part Number: DS280DF810
Hi !
We have a DS280DF810EVM debug board.
1. Is it possible to synthesize the synchronization frequency using the external pulse generator applied to the Rx0 input to obtain test data at the output of the Tx0 channel with a transmission rate of 28.78125, 25.78125, 10.3125 Gbps and Prbs 31?
2. What should be the topology of the connection scheme?
3. What should be the frequency of the external pulse generator for these transmission rates?
Regards, Dmitry.