Part Number: TUSB501
Other Parts Discussed in Thread: TUSB522P, TUSB551
I have three question as follows;
[1] When I confirm Vcm-RX of three re-driver, which are TUSB501, TUSB522P and TUB551, Vcm-RX is different for each re-driver. Why is Vcm-RX different for each re-driver?
- TUSB501 : Vcm-RX = 3.3V
- TUSB522P : Vcm-RX = 0.7V
- TUSB551 : Vcm_RX = 0V
[2] Can TUSB501 and TUSB551 receive the correct swing voltage when Vcm-RX=3.3V (=Vcc) or Vcm-RX=0V (=GND)?
[3] Can customer place the resister as shown at the following figure? If yes, what is the range of resister?
Thanks
Tamio