Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: DS90UB953-Q1EVM, , ALP
Tool/software: Linux
Hi,
I have a setup that looks like this:
cmos sensor --> DS90UB953-Q1EVM --> DS90UB954-Q1EVM --> usb cable with TI ALP / I2C bus controlled with nvidia
I managed to write from the usb to the three components (cmos+SerDes) but can't read
Also, I can read and write to SerDes on I2C bus
The problem is that I have only succeeded to read by I2C bus from CMOS but I can't write through I2C
I don't understand how it is possible that I can read but not write..
Is it the EVM Bug or I just need to change something in the way I sens the command?
Dorin