Part Number: TUSB1044
Other Parts Discussed in Thread: , TUSB1002, TUSB1002A
Hi,
I am trying to use TUSB1044 for USB3.1 signal conditioning with long passive USB type-C cables.
I plan to use TUSB1044 pin configured because I want to use captive USB cables and control by myself what set of pairs I am using.
My application includes also another redriver for DisplayPort, and I want to use the same device for both (with different configurations, of course)
To check the different configuration sets I have a TUSB1044RNQEVM. I am making tests with minimum cable lengths just to check the configurability of the direction of the redrivers.
I have been able to use seamlessly the ports TX1 and RX1 (DIR1/DIR0/CTL1/CTL0/FLIP = L/L/L/H/L and L/H/L/H/H). (See page 49 of TUSB1044 datasheet)
But I would like to use the ports TX2 and RX2 (DIR1/DIR0/CTL1/CTL0/FLIP = L/L/L/H/H or L/H/L/H/L) but the USB3 device I connect is not recognized.
TX2/RX2 ports should work exactly as TX1/RX1 ports or I am missing something?
JFI, the USB3.1 device I am using for the tests is a USB3 Loopback tester from PassMark. It is connected via a USB Type-C to USB micro B cable. I am taking into considerantion the orientation of that Type-C connection because only a set of RX/TX pairs ends in the microB end.
Regards,
Luis Jimenez