Part Number: DS90UH940N-Q1
Other Parts Discussed in Thread: DS90UB940-Q1
Hi,
I have a question.
In DS90Ux940 or DS90Ux940N, the color space conversion from RGB to YUV is possible,
and the register value is written in "Table 9. CSI-2 Output Data Formats".
In the YUV422 8-bit output, the register value of 0x6B [3: 2] IFMT is described as "00",
and it seems that RGB input is assumed.
If I want to output YUV422 8bit without color space conversion with YUV422 input,
is there a problem with 0x6B [3: 2] IFMT setting "00"?
Best regards