Part Number: TUSB2077A
Hi Team,
Would you advise that although it is the specification of RESET terminal (6Pin),
There is a description of the reference circuit: From P. 11 of sllu190.pdf, it is composed of
RC of 15 kΩ and 0.1 uF, and it is calculated to be 1.5 ms, but it is on the data sheet
(tusb 2077 a. Pdf: P. 5) According to the description of the recommendation is 100us to 1ms.
It is a circuit that does not comply with the specifications, but is it not particularly strict?
Please tell me if there is a place that you have to keep as a specification.
Thanks
Best regards,
Shidara