Part Number: TUSB1046-DCI
Other Parts Discussed in Thread: TPS65982, TUSB1046EVM, TPS65981, HD3SS460, TPS65981EVM, DP-EXPANSION-EVM
Hi
I want to have a dongle to take the DP source output from a laptop and send it through a USB-C cable to a USB-C only monitor.
Just wanted to confirm that the TUSB1046-DCI could do this.
The application will also need USB2.0 for touch input from the monitor to the laptop.
I've looked through the TUSB1046EVM and it looks almost suitable but it uses the TPS65982, which I would prefer not to use as it is only in BGA package.
Would the TUSB1046-DCI would be able to do this on its own, without any other chips, or would I need to use a USB-C controller such as the TPS65981?
Thanks