Part Number: TUSB8041
Hi Guys
Our customer found that the our TUSB8041A power loss is too high. Just to verify if their application is correct. Their system board input is 42V, which is not our device input. Their operating system is Android8.1, 42V power supply, TUSB8041A is connected to the system's usb3.0 host, and the four ports of TUSB8041A are not connected to any usb device.
(1) When the system is running:
If the sys node power/control of usb3.0 corresponding to TUSB8041A is set to auto (allowing the hub to automatically sleep), the input current of the system is about 80mA;
If the sys node power/control of usb3.0 corresponding to TUSB8041A is set to on (hub is not allowed to sleep automatically), the input current of the system is about 100mA.
From the above results, if set to auto, the hub should be automatically dormant.
(2) When the system is standby:
When the TUSB8041A is powered by V3.3 and V1.1, the input current of the system is approximately 30mA(System input is 42V);
When the TUSB8041A is powered off V3.3 and V1.1, the input current of the system is approximately 27mA(System input is 42V);
so if we calculate it by 42V, the power loss gap is around 126mW. so our device is about 120mW power loss at standby mode? could you help us check the schematic whether our system is something wrong? I will send you the schematic by email.
Thanks
-Pengfei