Part Number: DS90UB954-Q1
Dear *,
how much current can DS90UB954 drive from LOCK and PASS pin to direct drive a LED? Or do we need to add MOSFET?
Best Regards,
David.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Dear *,
how much current can DS90UB954 drive from LOCK and PASS pin to direct drive a LED? Or do we need to add MOSFET?
Best Regards,
David.
Hi David,
The current the DS90UB954 drives from the LOCK and PASS pins depends on the I/O voltage. Since the LOCK/PASS can be considered as GPIO’s, they are themselves driven by LVCMOS which can either be 1.8V or 3.3V.
For 1.8V, the output short circuit current would be 25 mA. For 3.3V, the output short circuit current would be 40mA. Since the LOCK and PASS drive the LED directly, you wouldn’t need a MOSFET.
For further reference, check pages 12 and 13 of the datasheet for current information: http://www.ti.com/lit/ds/symlink/ds90ub954-q1.pdf
Check page 31 of the user’s guide for a schematic of the LOCK/PASS LED configuration: http://www.ti.com/lit/ug/snlu223/snlu223.pdf
Best regards,
Liban H.