This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: Two-way Camera Input Application

Part Number: DS90UB936-Q1

Hi,

I have some questions in using DS90UB936Q1.

Does DS90UB936-Q1 support two cameras? Both LVDS are 1080P@30, 1080P is 2MP

I saw DS90UB954 also supported it, but it seems more expensive.

thanks,

  • Hello Wu,

    It depends on the actual data rate requirement which varies based on the color depth (bits per pixel) of your imager and the imager blanking, but for "typical" automotive imagers yes this should be doable with 936.

    Best Regards,

    Casey