This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: 4K DP1.2 over 20 meter

Expert 4655 points

Part Number: SN75DP130

Hi,
Customer is asking whether SN75DP130 is recommended for cable length up to 20m. Protocol is DP1.2, 4k.
Would you recommend other ICs?

Thanks & BR,
KF

  • KF

    Do you have a block diagram? What is the insertion loss of the cable? 

    For DisplayPort, TI has two solutions:

    DP139 is a limited re-driver which the transmitter provides its own SWING and Pre-emphasis, different from the DP source SWING and Pre-emphasis.

    DP142 is a linear re-driver which the transmitter does not have its own SWING and Pre-emphasis.

    Either one of them can be used depends on the system application requirement.

    They can order a EVM and use it to evaluate the cable.

    Thanks
    David