Part Number: TPD4E05U06
Dear team:
Does TPD4E05U06 support DP1.2?
Thanks!
Regards!
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Could you confirm the data rate for DP1.2?
Hi Cameron:
The DP1.2 single Lane is up to 5.4Gbps.
The line capacitance of TPD4E05U06 is 0.5pF,what data rate can it support? How much different data rates can 0.42pf and 0.5pf support?
Thanks!
Hello,
0.5pF can support 5.4Gbps. However in signal integrity it is all about loss budget. 0.5pF, according to the insertion loss graph in the datasheet, gives ~1.5dB of loss. Therefore if your trace and connectors do not give you more than ~1.5dB of loss then you have not exceeded your loss budget of 3dB for the system and can use this part.